Hi, I want to create a project with S32k324 based on RTD3.0 +FreeRTOS 10.5.1+Tcpip_stack1.0.3, and there is a problem that if the TCPIP use Freertos did lead to errors after making files. But when TCPIP didn't use Freertos, there weren't any problems. But it runs normally with FreeRTOS in the same way on the S32K344 .
Q:
1. Based on the above phenomenon, could it be that some configurations were overlooked in the project?And how to solve this problem?
2. Since the S32k324 has dual cores, and there're two core projects generated when I create the project, so I want to know that if I want to use FreeRTOS in each core project, should I intall the freeRTOS separately? And is there any examples of how to use S32k324 dual cores ?