S32K324 Crypto returns CRYPTO_RET_OPERATION_TIMEOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K324 Crypto returns CRYPTO_RET_OPERATION_TIMEOUT

1,231 Views
Faker
Contributor II

Hi,

I refer to the demo of Crypto_SymmetricPrimitives_S32K44 to use S32K324's Crypto module, but it can't run it correctly. I trace the code to find that it is timeout in the function of Hse_Ip_ServiceRequest.

/* Send the request to HSE driver */
HseResponse = Hse_Ip_ServiceRequest(u8MuInstance, u8MuChannel, pHseIpReq, pHseSrvDescriptor);
/* Translate the message received from HSE to a Std_ReturnType value */
RetVal = Crypto_Hse_TranslateHseResponse(HseResponse);

RetVal is the value of CRYPTO_RET_OPERATION_TIMEOUT. So I don't kown what the probelm is.

Are there any configurations that affect this function?

 

0 Kudos
Reply
1 Reply

1,197 Views
VaneB
NXP TechSupport
NXP TechSupport

H i @Faker 

To be able to run the example, you need to have installed the HSE FW.

As you are having a timeout at Hse_Ip_ServiceRequest, which means that is expecting the response of the HSE and is not getting it.

Please make sure to have installed the HSE FW before running the example code.

 

B.R.

VaneB.

0 Kudos
Reply