S32K322 Low power Wakeup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K322 Low power Wakeup

1,083 Views
vinaykl
Contributor III

Hello Team,

I had migrated the low power mode project from S32K344 to S32K322. But during Power Initialization it is stopping the execution. Kindly find the project files added with this query. Please let me know what steps I had missed. 

0 Kudos
Reply
3 Replies

1,063 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @vinaykl,

I am unable to test the project, since we only have the evaluation boards as reference, but does execution stop in line 97 (Power_Ip_Init)? 

In your design, could you confirm if the V15 supply is taken from de FS26/SBC 1.5V regulator?

 

Julin_AragnM_1-1751474489812.png

In the S32K344 EVB, if jumper J31 is set at default (1-2), this setting should be disabled:

Julin_AragnM_2-1751474524002.png

Other than that, I don't see anything necessarily wrong in the configuration or code, it seems to be the same as the provided examples.

Best regards,
Julián

0 Kudos
Reply

1,037 Views
vinaykl
Contributor III

Hi Julian,

Thank you for the response. I really appreciate your reply.

I have checked in our schematic V15 is connected to FS26_CORE. 

And whatever we have shared with you is perfectly working in S32K344 EVK and we don't have any problem there. 

Only when we migrated the project configuration and files from S32K344 to S32K322 we are facing this issue. The execution stops at Initialization of PowerInit(). 

Any other solution if available will be truly appreciated.

Regards,

Vinay

0 Kudos
Reply

1,031 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @vinaykl,

Could you share inside what function from Power_Ip_Init is the hard fault happening?

There could also be hardware issues that I'm unable to replicate because of the custom design. Please confirm if you've followed the hardware design guidelines from the HW Design Package.

Best regards,
Julián

0 Kudos
Reply