S32K314: try to build a project with freertos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314: try to build a project with freertos

Jump to solution
2,163 Views
cuiru_huaqin
Contributor II

Hi,sir:

I want to build a s32k314 project with freertos, but I can not find the "components library" .

"components library" like this:

cuiru_huaqin_0-1662108475049.png

the software i had installed:

-IDE: S32DS.3.5_b220726_win32.x86_64.exe
-RTD: SW32_S32DS_OfflineDevPack_3.5.0_D2207.zip

SW32K3_RTD_4.4_2.0.1_DS_updatesite_D2207.zip
-FreeRTOS: SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip

0 Kudos
Reply
1 Solution
2,110 Views
cuiru_huaqin
Contributor II

hi,all:

the question has been resolved, please folw the next steps.

cuiru_huaqin_0-1663292477206.pngcuiru_huaqin_1-1663292501999.pngcuiru_huaqin_2-1663292544397.png

cuiru_huaqin_3-1663292611475.png

cuiru_huaqin_4-1663292646977.png

cuiru_huaqin_5-1663292691173.png

cuiru_huaqin_6-1663292707435.pngcuiru_huaqin_7-1663292721994.pngcuiru_huaqin_8-1663292739762.pngcuiru_huaqin_9-1663292753381.pngcuiru_huaqin_10-1663292766383.pngcuiru_huaqin_11-1663292780452.pngcuiru_huaqin_12-1663292799960.pngcuiru_huaqin_13-1663292813156.png

View solution in original post

0 Kudos
Reply
4 Replies
2,111 Views
cuiru_huaqin
Contributor II

hi,all:

the question has been resolved, please folw the next steps.

cuiru_huaqin_0-1663292477206.pngcuiru_huaqin_1-1663292501999.pngcuiru_huaqin_2-1663292544397.png

cuiru_huaqin_3-1663292611475.png

cuiru_huaqin_4-1663292646977.png

cuiru_huaqin_5-1663292691173.png

cuiru_huaqin_6-1663292707435.pngcuiru_huaqin_7-1663292721994.pngcuiru_huaqin_8-1663292739762.pngcuiru_huaqin_9-1663292753381.pngcuiru_huaqin_10-1663292766383.pngcuiru_huaqin_11-1663292780452.pngcuiru_huaqin_12-1663292799960.pngcuiru_huaqin_13-1663292813156.png

0 Kudos
Reply
2,129 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @cuiru_huaqin,

Please follow the release notes of the FreeRTOS extension:

danielmartynek_0-1662532639827.png

 

Thanks,

BR, Daniel

0 Kudos
Reply
2,115 Views
cuiru_huaqin
Contributor II

Hi,sir:

  I have re-installed the software step by step according to the release notes(SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204_ReleaseNotes),but i still can not find where can add the freertos.

cuiru_huaqin_0-1663145812182.png

may be there is something that i don not know.

0 Kudos
Reply
2,156 Views
cuiru_huaqin
Contributor II

cuiru_huaqin_0-1662109617024.png

so, if there is another way to add the freertos code?

0 Kudos
Reply