I am using 314 chip, when burning the program, I found the problem in the picture, may I ask if there is a solution?
Solved! Go to Solution.
Hi
This issue has been fixed in S32K3 RTD 4.0.0.
Sorry for the inconvenience we bring you!
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
This issue has been fixed in S32K3 RTD 4.0.0.
Sorry for the inconvenience we bring you!
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks for your reply, it is indeed the problem here, and if it is changed, it will be successfully burned and the program can run normally. In order to avoid other unpredictable problems in RTD3.0.0 version, I would like to change it to RTD4.0.0 now, could you please provide the download link, can S32DS3.5 directly install RTD? If not, Do you need to uninstall RTD3.0.0 first? Please provide the installation operation sequence, thank you!
As far as I know, it is not possible to install multiple S32K3 RTD versions simultaneously in S32SD v3.5.
If you only need to use S32K3 RTD 4.0.0, please uninstall S32DS v3.5 and reinstall. If you don't find S32K3 RTD 4.0.0 in S32DS Extensions and Updates, please download the Offline Package and offline install it: S32K3 Standard Software->Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M->S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0
If you need to use multiple S32K3 RTD versions at the same time, the current recommendation is to install S32DS v3.5 with multiple paths, such as S32DS.3.5_S32K3RTD400 and S32DS.3.5_S32K3RTD300.