S32K314 app jump to bootloader question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 app jump to bootloader question

Jump to solution
3,271 Views
Faith-Herio
Contributor III

hellow,I encountered a rather tricky problem. I am using BootLoader+APP mode on S32K314. The same code works fine when the BootLoader jumps to the APP, but it triggers a hard fault when the app jumps back to the BootLoader. During debugging, I found that there was an error in setting up the stack. I can't think of a good solution for this issue and would like to ask if anyone has any suggestions?

The code and the values of the variables look like this:

 

    addr =0x00400000
    static void (*jump_to_bootloader)(void);
    static uint32_t stack_pointer;
    uint32_t appEntry, appStack;
 
    appStack = *(uint32_t *)(addr + 4096);
    appEntry = *(uint32_t *)(addr + 4096 + 4);
   
    jump_to_bootloader = (void (*)(void))appEntry;
    stack_pointer = appStack;
  
    S32_SCB->VTOR = (uint32_t)addr;
   
    __asm volatile("MSR msp, %0\n" : : "r"(stack_pointer) : "sp");
    __asm volatile("MSR psp, %0\n" : : "r"(stack_pointer) : "sp");
   
    jump_to_bootloader();
 
0 Kudos
Reply
1 Solution
3,244 Views
Faith-Herio
Contributor III
0 Kudos
Reply
4 Replies
3,114 Views
shuaige
Contributor I

hello ,can you teach me how to address this question?Thank you?Why not jump?

0 Kudos
Reply
2,395 Views
Faith-Herio
Contributor III

Note to check if the RTOS is used. If RTOS is used, pay attention to the usage of the MSP and PSP registers before jumping. If the boot loader does not apply RTOS, you need to change your stack usage to the MSP register. Similarly, if the RTOS is used in the APP or BOOT, you need to change your main stack to the PSP before jumping.

0 Kudos
Reply
3,245 Views
Faith-Herio
Contributor III

已解决

0 Kudos
Reply
2,393 Views
Faith-Herio
Contributor III

Note to check if the RTOS is used. If RTOS is used, pay attention to the usage of the MSP and PSP registers before jumping. If the boot loader does not apply RTOS, you need to change your stack usage to the MSP register. Similarly, if the RTOS is used in the APP or BOOT, you need to change your main stack to the PSP before jumping.

Tags (1)
0 Kudos
Reply