S32K314 LpUart interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 LpUart interrupt

668 Views
abhijith_r
Contributor III

Hi,

I am using S32K314 board, in our project we are connecting to a Modem in which we want to enable interrupt and read the bytes received in the UART. I am using Lpuart_Uart_Ip_AsyncReceive but I don't know the exact number of bytes that receiving through my AT commands. How to implement interrupt for a normal modem connection?

0 Kudos
Reply
1 Reply

652 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

You need to use the LPUART IDLE function. Maybe you can refer to the discussion in The S32K312 UART+DMA+IDLE No matter which UART sends, data is sent as 0

That project implement "UART receive indefinite length data".


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply