S32K314 DataFlash emulates EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K314 DataFlash emulates EEPROM

1,733件の閲覧回数
Danny_Wu
Contributor I

Hello,

According to the description in Section 20.5.5 of S32K3XXRM.pdf, S32K314 supports DataFlash emulated EEPROM, but this part is more general.
Where can I get the detailed information of EEPROM emulation and the sample project for S32K314?

0 件の賞賛
返信
1 返信

1,723件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

On this device there EEPROM is emulated by SW in the data flash. For understanding the principle I could recommend following appnote (although written for different platform, the principle is the same):
https://www.nxp.com/docs/en/application-note/AN4868.pdf

Driver and example project you may find in S32DS, it is called Fee_Example_S32K3xx.

In the installation directory, you may also find user manual for Flash EEPROM emulation driver:
c:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_10\SW32K3_RTD_4_4_1_0_0_D2110\Fee_TS_T40D34M10I0R0\doc\

0 件の賞賛
返信