S32K312NHT0MPAST SBC question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312NHT0MPAST SBC question

2,421 Views
hyjung
Contributor II

Hi team

The customer is looking for an SBC that will only supply adequate power to the S32K312NHT0MPAST.
Is UJA1169 possible??
If so, how do you handle unused pins (ex. CAN Tx/Rx, CANH, CANL) because only simple power is used?

Thanks.

0 Kudos
Reply
3 Replies

2,393 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello hyjung,

I hope all is great with you. Thank you for using the NXP communities.

Have you considered the FS26 - Safety System Basis Chip?

Such SBC is designed to work with the devices listed below:

 

diazmarin09_0-1687540916101.pngdiazmarin09_0-1687540916101.png

 

I hope this information helps.

Regards,

David

0 Kudos
Reply

2,343 Views
hyjung
Contributor II

Thanks reply.

 

I am inquiring because we need an IC for simple power supply, not FS26 / 23.

thank you.

0 Kudos
Reply

2,334 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

Thank you for using the NXP community.

I do recommend reviewing the S32K3 evaluations boards as a reference for your design.

As you noticed, all the solutions include a Safety SBCs (FS26) which is highly recommended to supply your MCU. The SBC or PMIC performs observations and control functionalities that are essential to fulfill some related functional safety requirements.

diazmarin09_0-1688146108795.pngdiazmarin09_0-1688146108795.png

 

I hope this information helps.

Regards,

David

0 Kudos
Reply