S32K312 without jlink or reset the program stop runing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 without jlink or reset the program stop runing

1,359 Views
binZhang01
Contributor III

When I used S32DS to create the S32K312 project, the first time I burned the program, it ran normally, but when I tried to power on or reset it, the program stopped running.

 

 

binZhang01_0-1715332566640.png

 

S32K3 

#S32DS

 

0 Kudos
Reply
1 Reply

1,335 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to the discussion in If I don't give s32k312 delay, the CAN stop during operation


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply