S32K312 without jlink or reset the program stop runing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 without jlink or reset the program stop runing

1,348件の閲覧回数
binZhang01
Contributor III

When I used S32DS to create the S32K312 project, the first time I burned the program, it ran normally, but when I tried to power on or reset it, the program stopped running.

 

 

binZhang01_0-1715332566640.png

 

S32K3 

#S32DS

 

0 件の賞賛
返信
1 返信

1,324件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to the discussion in If I don't give s32k312 delay, the CAN stop during operation


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信