S32K312 broken

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 broken

1,765 Views
NamNam
NXP Employee
NXP Employee

Hi S32K312 team,
I broke 2 boards S32K312 EVB Q172 within 3 months.
All of them have the same phenomenon that the source IC FS26 is very hot, which can burn my finger if touched. The computer still detects the COM port, but uploading the code from the S32DS fails.

The resistance between VDD_HV_A_MCU and GND is only 6 ohm. We have J18 as a 3.3V or 5V selector jumper for the MCU power. I removed it so there is no supply power to the MCU. Then the IC FS26 is not hot. I suspect that either the S32K312 IC is dead or the voltage stabilizer capacitors for the 3.3V pins have failed. After gradually removing the capacitors C16, C114, C101, C99, C100, C3857 and U5 ... I determined that IC S32K312 is exactly the cause of the hot source FS26. Both board broke while I was running my code, it worked fine a long time ago with this code. No problem with power via USB port and DC12V port.
Notice that the board failures came when I was using the connection to a hat board (add onboard) plugged in. But I have connected the add-on board many times before. It has an antenna that reads NFC tags. Could a strong electromagnetic field damage the IC?. I'm not sure that's the reason. Just wanted to provide enough information so that we do not miss any clues.

Any questions or suggestions to determine the reason for the board failure is high appreciated.

Currently S32K3123 EVB Q172 is very difficult to find on the market, so it is very difficult for me at work.
Thank you.

0 Kudos
Reply
2 Replies

1,738 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you specify what is used 'hat board' you are mentioning? According your description it seems rather as shortcut on certain MCU power supply rail. I suppose you are plugging your hat board when the EVB is out of power.

0 Kudos
Reply

1,700 Views
NamNam
NXP Employee
NXP Employee
0 Kudos
Reply