S32K312 UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 UART

1,280件の閲覧回数
lua40927
Contributor III

Hello
I would like to ask if there are any other LPUART interrupts besides the 4 shown below?

LPUART.png

I want a receive interrupt to occur when the UART receives a character
Then store the characters in the Call back function

 

タグ(1)
0 件の賞賛
返信
1 返信

1,254件の閲覧回数
RomanVR
NXP Employee
NXP Employee

Hello @lua40927.

Those are the only events which trigger the interrupts. However, you can configure the receive buffer size to meet your specific requirements, as shown in the below image:

2025-02-04_16-01-35.jpg

I recommend to trying the "Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300" to familiarize yourself with the UART driver and APIs, which are useful to configure the Rx buffer to trigger the Rx_Full event with one character and access to the configured callback. Also, please refer to de S32K3XX Reference Manual Rev. 9 for more information about the LPUART module.

Please let me know if this was helpful.

- RomanVR.

Best Regards!
0 件の賞賛
返信