Hi
Have you already referred to this example? Example S32K312 SPI Transmit & Receive Using DMA DS3.5 RTD300
Note that the buffer needs to be placed in the NON CACHEABLE memory section.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I have referred to this example? Example S32K312 SPI Transmit & Receive Using DMA DS3.5 RTD300.
Waveform measurement, as shown in the diagram below.
CS and MOSI are kept at a high level in the diagram, while SCLK and MISO are kept at a low level.
Seems that you forget configure Dma Hardware Channel and Dma Mux Source in Rm component.
Please refer to the settings of Example S32K312 SPI Transmit & Receive Using DMA DS3.5 RTD300. :