S32K312 Reset_Handler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Reset_Handler

1,352 Views
LILV
Contributor II

I have a 12V project using the S32K312 chip. However, during the operation, due to the system not being in sleep mode, the battery voltage gradually dropped from 12V to 3V. Then, I tried to charge the battery, but all functions disappeared. Even after a power-off and power-on, the functions did not recover. I try to attach this chip and discovered that the program had stucked in the Reset_Handler step.

What could be the reason for this?

屏幕截图 2026-02-12 144931.png

 

Tags (2)
0 Kudos
Reply
4 Replies

1,330 Views
LILV
Contributor II

This is the startup file.

0 Kudos
Reply

1,322 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Can you show me where is it stuck in the startup?

You should see it in the disassembly.

 

 

 

0 Kudos
Reply

1,191 Views
LILV
Contributor II

sorry and I can only see the fault information provided to me by S32DS.

屏幕截图 2026-02-12 144931.png

0 Kudos
Reply

1,335 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @LILV,

In what loop is it stuck?

Can you share the startup code and the disassembly?

 

Thank you,

BR, Daniel

0 Kudos
Reply