S32K312 LPI2c1 is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K312 LPI2c1 is not working

1,822 次查看
rekhak
Contributor I

Hi Team,

I am working on I2c Bringup on S32K312 chip.

i have made below configurations :

LPI2C0 - Slave configuration - working

LPI2C1 - Master configuration - not working

Configurator changes:

rekhak_0-1747739212421.pngrekhak_1-1747739248157.png

 

AIPS_SLOW_CLK is the I2c module clock - it is configured as 20MHz.

OS ISR for master is configured - 

rekhak_2-1747739332750.png

 

Problem Statement:

" both I2c SCL and SDA are pulled high always"

even though i can see the I2c_init is successful and there were few write commands also passed successfully, still there is no clock / data seen on bus.

Please suggest here.

 

Thanks,

Rekha

 

0 项奖励
回复
5 回复数

1,760 次查看
rekhak
Contributor I

i could figure out solution, there was one configuration missing. post that change  i am able to see the start bit on bus but then bus goes idle. throws error callback with arbitration error.  Need your help to resolve this issue.

0 项奖励
回复

1,750 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @rekhak 

The arbitration error you are seeing usually means that your device lost control of the I2C bus, which can happen if more than one master tries to communicate at the same time.

Do you have multiple master devices on your I2C bus? If so, it is important to make sure they are not trying to send data at the same time, as that can cause conflicts.

Also, it is a good idea to double-check that your master device is waiting for the bus to be idle before starting any communication. This helps avoid collisions and keeps everything running.

0 项奖励
回复

1,779 次查看
rekhak
Contributor I

Slave configurations :

rekhak_0-1747807274697.png

 

0 项奖励
回复

1,794 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @rekhak 

I am afraid I am not familiar with Vector DaVinci, so my observations are based on a comparison between the S32DS configurations and the S32K3xx Reference Manual information.

The LPI2C configurations appear generally correct. However, I have one observation regarding the interrupt configuration. Specifically, for the ISR Interrupt Priority parameter, you assigned a value of 144. According to the S32K3xx Reference Manual, there are 16 priority levels, which are configurable using 4 bits in the IRQn fields of the NVIC IPRn registers. Furthermore, based on the NVIC_SetPriority() function, only the upper 4 bits of the 8-bit priority field are implemented, meaning that only values from 0 to 15 are valid.

VaneB_0-1747764901785.png

For clarity and maintainability, it is recommended to use values within the 0–15 range directly.

Additionally, could you please confirm whether the same configuration works correctly for LPI2C0? From what I can see, there does not appear to be an issue with the current configuration, so verifying its behavior on LPI2C0 could help us rule out a direct issue with LPI2C1.

 

BR, VaneB

0 项奖励
回复

1,779 次查看
rekhak
Contributor I
HI VaneB,
Thank you for your quick response .
LPI2C0 is configured as slave , priority for slave channel is also given as 144 and it works without any issue.
标记 (1)
0 项奖励
回复