S32K312 IIC CONFIG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 IIC CONFIG

1,467 Views
chenyh
Contributor II

f70f499e76eb7c7826cabe0297054a1.png5f06e06d5a44fe2ebd4607f66987a93.pngI want to know what exactly the configuration of IIC in the box represents, and now I don't know how to modify it, and then why the SCL of IIC should be configured as the input and output mode. I remember that under normal circumstances, SCL only needs to configure the output mode, I hope someone can give me an answer, thank you very much

0 Kudos
Reply
1 Reply

1,440 Views
RomanVR
NXP Employee
NXP Employee

Hi @chenyh

The timing parameters that you're watching in configuration tools are required for the proper operation of the LPI2C controller accordingly to the operation mode.

Firstly, the preescaler is a frequency adjustable divisor to divide the module's operation clock frequency and. It can take a value of 1, 2, 4, 8, 16, 32, 64 and 128.

Find attached the table from section 71.7.1.13 Controller Clock Configuration 0 of S32K3xx Reference Manual, Rev. 9 where these timing parameters are explained.

RomanVR_0-1734125439231.png

RomanVR_1-1734125447368.png

I also attach Table 462 of section 71.6 of S32K3xx Reference Manual, Rev. 9 which includes some examples of timing configurations for different I2C operations modes:

RomanVR_2-1734125468539.png

RomanVR_3-1734125477834.png

About SCL modes, although normally SCL line is used as unidirectional, some slave devices have the need to hold the clock line low in order to tell the master to wait until the information received is processed, therefore the need of a bidirectional SCL line.

For more detailed information please refer to S32K3xx Reference Manual, Rev. 9 available at S32K3 Microcontrollers for Automotive General Purpose.

If you have more doubts, feel free to share them.

- RomanVR.

Best Regards!
0 Kudos
Reply