S32K312 HSE CLK & UTEST write error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K312 HSE CLK & UTEST write error

957 次查看
David2024
Contributor II

MCU:S32k312; MCAL:MCAL4.0; FXOSC:24MHz.

when config HSE clock to 120MHz and write data to UTEST(0x1B00 0000), then there will be a Hardfault.

when config HSE clock to 60MHz, we can write the data to UTEST successful.

We didn't have this problem when we used MCAL1.0 before.

标记 (1)
0 项奖励
回复
1 回复

935 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

What is version of RTD?
Have you referred to the methods described in chapter 9.3. Improve performance of Secure Boot Application note v0.1.1.0?

IMPORTANT: The 120MHz cannot be set by software directly. It won’t work. Please check the following post. It has information related to this problem: HSE provides RSP_NOT_SUPPORTED response 


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复