Hello, I have a question. I want to realize the synchronous acquisition of 3 AD channels by two ADCs, that is, the acquisition of 6 AD channels within 3 sampling cycles. Can it be realized?
Is it possible to use one PWM to trigger BCTU and write two different ADC channels in the list? Do the two ADCs trigger conversions at the same time or do they convert in sequence according to the list?
Or is it necessary to implement two PWM as trigger signals? Does using two PWM as trigger signals require a trigger signal priority wait? That is, new trigger signals are not received until the conversion of the ADC triggered by the previous trigger signal is complete, even if they are not triggered by the same ADC?
In addition, does watermark mean the trigger signal priority after BCTU receives multiple trigger signals at the same time?
已解决! 转到解答。