S32K312 ADC0_P6 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 ADC0_P6 problem

1,176 Views
coo
Contributor I

S32K312 보드를 사용하고 있습니다.
ADC0을 사용하려고 노력하는 것이 ADC0_P6 기본이 아닙니다.
12 비트가 있고, 하드웨어적으로 괜찮은 것을 확인했습니다.
설정은 다른 기능과 동일합니다.

이 문제가 발생하는 이유를 알 수 있습니까?

image.png

S32K312.pngimage.pngimage.png다른 포트와 다르게 설정해야 할까요?

 

Tags (1)
0 Kudos
Reply
1 Reply

1,155 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please use a voltmeter to measure whether the voltage of ADC0_P6 pin is the same as other ADC input pins.
Please check whether the software configuration of ADC0_P6 is the same as other channels.
Which board are you using? ADC0_P6 of S32K312EVB-Q172 is connected to TOUCH_ADC_A by default.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply