S32K3_pinout mapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3_pinout mapping

4,513件の閲覧回数
michael_gao
Contributor II

Dear NXP

I download NXP S32K3 pinout mapping.

I can't see S32K322 & S32K314 & S32K324.

Maybe the name is wrong.

Can you provide the correct pinout mapping ?

 1MB/2MB Single Core2MB Dual Core4MB Single and Dual Core8MB Dual/Triple Core
PackageK311K312K322K342K314K324K344K328K338K348K358
48LQFPS32K311_48LQFP          
100HDQFPS32K311_100hdqfpS32K312_100hdqfpS32K342_100hdqfpS32K342_100hdqfpS32K314_100hdqfp      
172HDQFP S32K312_172hdqfpS32K342_172hdqfpS32K342_172hdqfpS32K344_172hdqfpS32K344_172hdqfpS32K344_172hdqfpS32K358_172hdqfpS32K358_172hdqfpS32K358_172hdqfpS32K358_172hdqfp
257BGA    S32K344_257BGAS32K344_257BGAS32K344_257BGA    
289BGA       S32K358_289BGAS32K358_289BGAS32K358_289BGAS32K358_289BGA
タグ(2)
0 件の賞賛
返信
6 返答(返信)

4,466件の閲覧回数
michael_gao
Contributor II

Dear Senlent

 

Sorry , Another question.

Is S32K342  different  from S32K344 ?

The same color have two reference part number.

"Pinouts with the same color indicate same pinout is used"

 

0 件の賞賛
返信

4,462件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@michael_gao

The pin map of S32K342 is the same as S32K344, but the memory size is different.

0 件の賞賛
返信

4,469件の閲覧回数
michael_gao
Contributor II

Dear Senlent

 

Thanks. I got it.

Because the color of green show S32K311, S32K312, S32K314.

Another color only show one part number.

It make me wonder.

Thank you for your support.

0 件の賞賛
返信

4,494件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@michael_gao

you can find all the pin map of S32K3 in S32K3xx Reference Manual 's attachments.

Also you can find below describtion:"Pinouts with the same color indicate same pinout is used"

Senlent_0-1733120256960.pngSenlent_0-1733120256960.png

 

0 件の賞賛
返信

4,479件の閲覧回数
michael_gao
Contributor II

Dear Senlent

 

So I think the document has a wrong.

I can't see S32K322_172,  S32K314_172 and S32K324_172.............

always S32K344_172.

Thanks.

0 件の賞賛
返信

4,475件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@michael_gao

"Pinouts with the same color indicate same pinout is used"

so"S32K322_172,  S32K314_172 and S32K324_172" pin map can refer to S32K344_172

0 件の賞賛
返信