S32K3 RTD Power reset api box does not change Power_Ip_Cfg_Defines value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 RTD Power reset api box does not change Power_Ip_Cfg_Defines value

1,934 Views
pb632146
Contributor V

pb632146_0-1742432926303.pngpb632146_0-1742432926303.png

 

pb632146_1-1742432942634.pngpb632146_1-1742432942634.png

I was trying to figure out why ticking the box did not enable the  Power_Ip_PerformReset() API and it seems that the define does not change. Why is this happening? Manually changing the define seems to work but it is a little annoying

0 Kudos
Reply
6 Replies

1,396 Views
ChowZJ
Contributor II

HI, @pb632146 

Have you found the cause? I am experiencing the same problem.

0 Kudos
Reply

1,913 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@pb632146

For example, you can click "change" to see the code is changed or not

Senlent_0-1742444608827.pngSenlent_0-1742444608827.png

 

0 Kudos
Reply

1,908 Views
pb632146
Contributor V

Yeah even in the update code section it shows that it doesnt change anything

pb632146_2-1742447131055.pngpb632146_2-1742447131055.png

 

pb632146_1-1742447056293.pngpb632146_1-1742447056293.png

 

I suppose this is more of a bug report than anything that the peripherals tab isn't translating properly to the code changes.

0 Kudos
Reply

1,904 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@pb632146

Could you please tell me the IDE and RTD version you're using, i will try to reproduce this problem and give you feedback from myside.

0 Kudos
Reply

1,880 Views
pb632146
Contributor V
ide 3.6 and rtd 5.0
0 Kudos
Reply

1,857 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@pb632146

You can see there is no such problem on myside.

Senlent_0-1742520291662.pngSenlent_0-1742520291662.png

 

0 Kudos
Reply