S32K3 MCU debug port secure with good ADKP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 MCU debug port secure with good ADKP

1,711 Views
Shaun666
Contributor II

Hello

I have an ECU with static ADKP for debug port, and I have previously connected to the ECU using the Lauterbach with the ADKP. but today, I try to debug  the ECU with same to previous script ,the Lauterbach feedback debug port secure. Do you have the same situation? I only have Lauterbach ,how can I stable connect to JTAG?

attached is the script of Lauterbach.

Tags (1)
0 Kudos
Reply
3 Replies

1,659 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am afraid I cannot provide solution without deeper knowledge what actually happened. Could you share some screenshots or logs?

@rweiss 

0 Kudos
Reply

1,641 Views
Shaun666
Contributor II

since I can't connect the MCU, so I have a screenshot only this. Do you have any method remove the ADKP if I connected the MCU with JTAG?

 

New Bitmap Image (3).bmp

0 Kudos
Reply

1,596 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am afraid on this device there is no mechanism how to unsecure the device in such cases when it is not known what actually happened.

0 Kudos
Reply