S32K3 Hardware Watchdog

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Hardware Watchdog

ソリューションへジャンプ
5,146件の閲覧回数
rexoplans
Contributor III

Does the S32K3 series microcontrollers have hardware timers or software timers? Or is the term SWT only used as a naming convention and referred to as software in name only? 

タグ(1)
0 件の賞賛
返信
1 解決策
5,100件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

As for software-wise or hardware-wise, are you referring as if you should be able to see the external reset signal being asserted?

Under the S32K3 reset sequences there are 3 types:

  • Power-ON Reset (POR)
  • Destructive Reset
  • Functional Reset

From the 3 types, the SWT module will generate a Functional Reset which is described as [Page 1205, S32K3xx Reference Manual, Rev. 6, 04/2023]:

"Leads all the communication peripherals and cores to reset. The communication protocols' sanity
is not guaranteed and they are assumed to be reinitialized after reset. The SRAM content, and
the functionality of certain modules, is preserved across functional reset."

As for the RESET_b pin, the following is described [Page 1222, S32K3xx Reference Manual, Rev. 6, 04/2023]:

"The RESET_b pin offers the following uses if you configure it for the reset functionality:

  • Acts as an external destructive reset source
  •  Acts as an indicator for the chip reset sequence for both functional and destructive reset sequences "

We may again be misunderstanding your request, if so we apologize.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,116件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Looking at the title and from your question, we assume you are asking the following:

"Does the S32K3 series microcontrollers have watchdog hardware timers or watchdog software timers?"

If so, as you are implying, it is a naming convention. Since the SWT has registers that need configurations, it is a module embedded inside the MCU itself that requires an initialization [Page 2749, Chapter 67.5, S32K3xx Reference Manual, Rev. 6, 04/2023]. This can also be seen under the SWT Block Diagram [Page 2747, S32K3xx Reference Manual, Rev. 6, 04/2023]:

DanielAguirre_0-1694452584378.png

Please, let us know.

0 件の賞賛
返信
5,113件の閲覧回数
rexoplans
Contributor III
"I actually couldn't explain the topic that confuses me exactly. Hardware-wise, I believe there is a Watchdog module, but when I tinkered with it a bit, it seemed to be just a timer. When the timeout value is reached, will the process of resetting the processor be done hardware-wise or software-wise?
0 件の賞賛
返信
5,101件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

As for software-wise or hardware-wise, are you referring as if you should be able to see the external reset signal being asserted?

Under the S32K3 reset sequences there are 3 types:

  • Power-ON Reset (POR)
  • Destructive Reset
  • Functional Reset

From the 3 types, the SWT module will generate a Functional Reset which is described as [Page 1205, S32K3xx Reference Manual, Rev. 6, 04/2023]:

"Leads all the communication peripherals and cores to reset. The communication protocols' sanity
is not guaranteed and they are assumed to be reinitialized after reset. The SRAM content, and
the functionality of certain modules, is preserved across functional reset."

As for the RESET_b pin, the following is described [Page 1222, S32K3xx Reference Manual, Rev. 6, 04/2023]:

"The RESET_b pin offers the following uses if you configure it for the reset functionality:

  • Acts as an external destructive reset source
  •  Acts as an indicator for the chip reset sequence for both functional and destructive reset sequences "

We may again be misunderstanding your request, if so we apologize.

Please, let us know.

0 件の賞賛
返信