S32K3 HSE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 HSE

1,932 Views
chenhuang
Contributor II

Hello All,

       There are some question for the GM HSE, would you please confirm 

  1. Which GM standards does NXP follow to develop the firmware? Would you give a list of the standards and the verion?
  1.  would you please fill the information.

 

(1)Does the HSM (including the firmware) meet all specifications as specified in CYS2300 - HSM Core Requirements? Does the HSM meet CYS2000, CYS3000,CYS4000, CYS9000, CYS2310, and chapter 8 of GB8001.   If 'No', please provide details in the 'Comments' field.

 

 

(2)Is an additional key use determination security flag (Verify_Only) implemented within the HSM for Key_<n> slots (KEY_1 – KEY_50) to restrict a keys usage to MAC verification only (not allowing MAC Generation) by setting this flag  set to "1"?

 

(3)Does HSM MacGen(t) or MacVerify(t) process taken less than 10us considering 16 byte of data? If No, please provide performance time for the commands.

(4)Does CMD_LOAD_KEY process taken less than 2ms?  If No, please provide performance time for the command.

(5)Is the HSM debugger port password checked every time HSM debug access is requested? Is the HSM debugger port locked after the micro resets? Is the HSM debugger port disabled after programming the HSM? Does unlocking the JTAG/Debug port of the micro not automatically unlock the debug port of the HSM?

 

(6)Do the CRY drivers meet all specifications as specified in CYS2300 - HSM Core Requirements? 

Does the CRY drivers meet CYS2000, CYS3000,CYS4000, CYS9000 and chapter 8 of GB8001.  

If 'No', please provide details in the 'Comments' field.

0 Kudos
Reply
1 Reply

1,864 Views
ChaoranYuan
Contributor I

Hi,

May I ask how to access the CYS2300 - HSM Core Requirements documents? I have searched for these GM security requirements files for a long time.

0 Kudos
Reply