S32K3 HSE FW Download

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 HSE FW Download

2,110件の閲覧回数
Zhiwei
Contributor II

@Haibing-Zeng Hi, According to 《HSE_DEMOAPP_S32K3X4_0_1_1_0_ReadMe》, this step is executed, as shown in Figure 3, and it is found that the bin file cannot be found. Please help to solve the confusion, thank you very much!

CatchDDC0(03-02-09-02-06).jpg

 

Catch74A7(03-02-09-02-07).jpg

CatchFDFB(03-02-09-02-07).jpg

  

タグ(1)
0 件の賞賛
返信
1 返信

2,091件の閲覧回数
NXF55009
NXP Employee
NXP Employee

Hi Zhiwei:

Your lauterbach T32 version may not work with HSE_DEMOAPP_S32K3X4_0_1_1_0.

Below is the flash bin file I found in the new version of T32(C:\T32\demo\arm\flash\long)

nxf55009_0-1646188313681.png

 

And the old version, which can only use HSE_DEMOAPP_S32K3XX_0_0_8_3.

nxf55009_1-1646188405486.png

I upload the S32K3x2.bin and S32K3x4.bin , you can try copy that to your folder, or use the HSE_DEMOAPP_S32K3XX_0_0_8_3 first for learning.

 

BR. 

Haibing.Zeng

 

0 件の賞賛
返信