S32K3 Fee moudle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Fee moudle

2,269 Views
hah31
Contributor II

I'm going working on Fee module config in S32K344 .

I config Feeblock in Fee module in EB and use Function Fee_Write to write something into,but I find the value just into Ram not Feeblock in DFlash which I want to write.

hah31_0-1730777078266.png

 

So I want to know how Fee_Write's to work. And other topic do you have some manual to introduce these Function? 

Tags (1)
0 Kudos
Reply
3 Replies

2,212 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is an example code, I would recommend to start with.

davidtosenovjan_0-1730911123069.png

 

2,188 Views
hah31
Contributor II

Hello,

         Thanks for your reply. Yes,I refer the example. Could I think Fee_Write actually is according to FeeBlockIndexNumber which I config in EB to write something , not according to detail physical Address?

 

BR

 

0 Kudos
Reply

2,247 Views
hah31
Contributor II

RTD Version is SW32K3_S32M27x_RTD_4.4_4.0.0_P24_DS_updatesite_D2405.zip

0 Kudos
Reply