S32K3 EB tresos29 problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 EB tresos29 problems

1,948件の閲覧回数
id9527
Contributor I

I want to use S32K3 + autosar,I can use the tool to generate some code, but make encountered some issues。T32_DIR=replace_t32_dir is invalid! so What should I do

id9527_0-1699336166638.png

id9527_1-1699336563470.png

 

 

thank you!

0 件の賞賛
返信
2 返答(返信)

1,912件の閲覧回数
CongDang
NXP Employee
NXP Employee

It's not issue with EBtresos.

T32_DIR needs to be defined with a path to Trace32 software that is used to debug with Lauterbach debugger.
So In this case you just need to search where T32_DIR is defined and replace that definition with a path that is valid on your PC.

0 件の賞賛
返信

1,702件の閲覧回数
harryoceana
Contributor II
I don't have a Lauterbach debugger and I can't install Trace32 software. What if I only use jlink debugging?
タグ(1)
0 件の賞賛
返信