S32K3 (Cortex-M7) Cache Handling Requirements for Flash Operations (Erase/Write) and Bootloader Jump

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 (Cortex-M7) Cache Handling Requirements for Flash Operations (Erase/Write) and Bootloader Jump

1,140 Views
yusupkhan241
Contributor III

Hi,

I am creating this thread as a follow-up to the previous discussion regarding flash erase/write issues:

https://community.nxp.com/t5/S32K/C40-Flash-Erase-Write-from-Bootloader-in-S32K311-Same-Flash/m-p/23...

The issue mentioned there has been resolved. However, I have some questions specifically related to cache usage on S32K3 devices.

  1. Is it possible to perform flash erase and write operations without using the cache module? Or is cache handling mandatory for reliable operation?

  2. If cache is required, what precautions should be taken during flash operations (erase/write)?

    • Do we need to explicitly clean/invalidate cache before and after operations?

    • Is there a recommended sequence to follow?

  3. What are the pros and cons of enabling cache in this context?

  4. I am using a bootloader + application setup. While jumping from bootloader to application, are there any mandatory cache-related steps (e.g., cache clean/invalidate, barriers, etc.) that must be performed?

Any guidance or recommended best practices for S32K3 (Cortex-M7) would be very helpful.

Thanks,

Yusup

0 Kudos
Reply
1 Reply

1,126 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Yusup,

On Cortex‑M7, there are D‑Cache and I‑Cache that operate on cacheable memory regions when enabled.

Whether a memory region is cacheable or not is configured in the core’s MPU.

In an S32DS IDE project, please refer to the linker file and system.c, where the MPU is configured and the I‑Cache and D‑Cache are enabled. Some memory regions are configured as cacheable, while others are configured as non‑cacheable.

 

1. Yes, it is possible. However, I do not see any reason to disable the cache. You would need to configure the regions where the flash driver operates as non‑cacheable, or disable the cache entirely.

2. The driver takes care of cleaning the cache if Mem Clean Cache After Load Access Code is set to 1. If the SRAM region where you copy the driver code is configured as non‑cacheable, you can set Mem Clean Cache After Load Access Code to 0.

3. Nothing special in this context. In general:
Pros: Cache greatly improves performance and reduces CPU stalls by keeping frequently used data and instructions close to the core.
Cons: Cache adds complexity and can cause data coherency issues.

4. Yes, it is good practice to clean and disable the cache. The startup code of the application will then reconfigure the MPU and re‑enable the cache. Also, refer to the S32K3xx Reference Manual, Section 3.8, Serialization of Memory Operations.

 

Regards,

Daniel

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-2358567%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ES32K3%20(Cortex-M7)%20Cache%20Handling%20Requirements%20for%20Flash%20Operations%20(Erase%2FWrite)%20and%20Bootloader%20Jump%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2358567%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%2C%3C%2FP%3E%3CP%3EI%20am%20creating%20this%20thread%20as%20a%20follow-up%20to%20the%20previous%20discussion%20regarding%20flash%20erase%2Fwrite%20issues%3A%3C%2FP%3E%3CP%3E%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32K%2FC40-Flash-Erase-Write-from-Bootloader-in-S32K311-Same-Flash%2Fm-p%2F2355746%23M58166%22%20target%3D%22_blank%22%3Ehttps%3A%2F%2Fcommunity.nxp.com%2Ft5%2FS32K%2FC40-Flash-Erase-Write-from-Bootloader-in-S32K311-Same-Flash%2Fm-p%2F2355746%23M58166%3C%2FA%3E%3C%2FP%3E%3CP%3EThe%20issue%20mentioned%20there%20has%20been%20resolved.%20However%2C%20I%20have%20some%20questions%20specifically%20related%20to%20cache%20usage%20on%20S32K3%20devices.%3C%2FP%3E%3COL%3E%3CLI%3E%3CP%3EIs%20it%20possible%20to%20perform%20flash%20erase%20and%20write%20operations%20without%20using%20the%20cache%20module%3F%20Or%20is%20cache%20handling%20mandatory%20for%20reliable%20operation%3F%3C%2FP%3E%3C%2FLI%3E%3CLI%3E%3CP%3EIf%20cache%20is%20required%2C%20what%20precautions%20should%20be%20taken%20during%20flash%20operations%20(erase%2Fwrite)%3F%3C%2FP%3E%3CUL%3E%3CLI%3E%3CP%3EDo%20we%20need%20to%20explicitly%20clean%2Finvalidate%20cache%20before%20and%20after%20operations%3F%3C%2FP%3E%3C%2FLI%3E%3CLI%3E%3CP%3EIs%20there%20a%20recommended%20sequence%20to%20follow%3F%3C%2FP%3E%3C%2FLI%3E%3C%2FUL%3E%3C%2FLI%3E%3CLI%3E%3CP%3EWhat%20are%20the%20pros%20and%20cons%20of%20enabling%20cache%20in%20this%20context%3F%3C%2FP%3E%3C%2FLI%3E%3CLI%3E%3CP%3EI%20am%20using%20a%20bootloader%20%2B%20application%20setup.%20While%20jumping%20from%20bootloader%20to%20application%2C%20are%20there%20any%20mandatory%20cache-related%20steps%20(e.g.%2C%20cache%20clean%2Finvalidate%2C%20barriers%2C%20etc.)%20that%20must%20be%20performed%3F%3C%2FP%3E%3C%2FLI%3E%3C%2FOL%3E%3CP%3EAny%20guidance%20or%20recommended%20best%20practices%20for%20S32K3%20(Cortex-M7)%20would%20be%20very%20helpful.%3C%2FP%3E%3CP%3EThanks%2C%3C%2FP%3E%3CP%3EYusup%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-2358626%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%20translate%3D%22no%22%3ERe%3A%20S32K3%20(Cortex-M7)%20Cache%20Handling%20Requirements%20for%20Flash%20Operations%20(Erase%2FWrite)%20and%20Bootloader%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-2358626%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3BYusup%2C%3C%2FP%3E%0A%3CP%3EOn%20Cortex%E2%80%91M7%2C%20there%20are%20D%E2%80%91Cache%20and%20I%E2%80%91Cache%20that%20operate%20on%20cacheable%20memory%20regions%20when%20enabled.%3C%2FP%3E%0A%3CP%3EWhether%20a%20memory%20region%20is%20cacheable%20or%20not%20is%20configured%20in%20the%20core%E2%80%99s%20MPU.%3C%2FP%3E%0A%3CP%3EIn%20an%20S32DS%20IDE%20project%2C%20please%20refer%20to%20the%20linker%20file%20and%20system.c%2C%20where%20the%20MPU%20is%20configured%20and%20the%20I%E2%80%91Cache%20and%20D%E2%80%91Cache%20are%20enabled.%20Some%20memory%20regions%20are%20configured%20as%20cacheable%2C%20while%20others%20are%20configured%20as%20non%E2%80%91cacheable.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3E1.%20Yes%2C%20it%20is%20possible.%20However%2C%20I%20do%20not%20see%20any%20reason%20to%20disable%20the%20cache.%20You%20would%20need%20to%20configure%20the%20regions%20where%20the%20flash%20driver%20operates%20as%20non%E2%80%91cacheable%2C%20or%20disable%20the%20cache%20entirely.%3C%2FP%3E%0A%3CP%3E2.%20The%20driver%20takes%20care%20of%20cleaning%20the%20cache%20if%20Mem%20Clean%20Cache%20After%20Load%20Access%20Code%20is%20set%20to%201.%20If%20the%20SRAM%20region%20where%20you%20copy%20the%20driver%20code%20is%20configured%20as%20non%E2%80%91cacheable%2C%20you%20can%20set%20Mem%20Clean%20Cache%20After%20Load%20Access%20Code%20to%200.%3C%2FP%3E%0A%3CP%3E3.%20Nothing%20special%20in%20this%20context.%20In%20general%3A%3CBR%20%2F%3EPros%3A%20Cache%20greatly%20improves%20performance%20and%20reduces%20CPU%20stalls%20by%20keeping%20frequently%20used%20data%20and%20instructions%20close%20to%20the%20core.%3CBR%20%2F%3ECons%3A%20Cache%20adds%20complexity%20and%20can%20cause%20data%20coherency%20issues.%3C%2FP%3E%0A%3CP%3E4.%26nbsp%3BYes%2C%20it%20is%20good%20practice%20to%20clean%20and%20disable%20the%20cache.%20The%20startup%20code%20of%20the%20application%20will%20then%20reconfigure%20the%20MPU%20and%20re%E2%80%91enable%20the%20cache.%20Also%2C%20refer%20to%20the%20S32K3xx%20Reference%20Manual%2C%20Section%203.8%2C%20Serialization%20of%20Memory%20Operations.%3C%2FP%3E%0A%3CBR%20%2F%3E%0A%3CP%3ERegards%2C%3C%2FP%3E%0A%3CP%3EDaniel%3C%2FP%3E%3C%2FLINGO-BODY%3E