S32K1xx PDB Trigger Input Source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1xx PDB Trigger Input Source

1,329 Views
Wupengfei2031
Contributor I

On page 1325 of the S32K-RM

PDB's register Status and Control register (PDB_SC) bit TRGSEL

The description is Refer to chip configuration details for the actual PDB input trigger
connections.

But I can't find any information about chip configuration details.

What can I do to find the related trigger input source?

0 Kudos
Reply
1 Reply

1,318 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Wupengfei2031

Figure 43-2. ADC0_PDB0 ADC Triggering scheme example

Senlent_0-1655883627362.png

Figure 19-3. Trigger interconnectivity (part 2 of 2: outputs 64-127)

Senlent_1-1655883781489.png

 

 

0 Kudos
Reply