S32K148EVB can't flash and debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148EVB can't flash and debug

998件の閲覧回数
devon1020
Contributor I

I use S32K148EVB via S32 Debug Probe to debug "hello" example in "Debug_Flsh" configuration

first i test Probe and EVB connection,

S32DS return "The board is not connected",

then i press reset switch and test connection again,

S32DS return "The board is connected", but display information seem like weird

"SoC IDCODE:0xFFFFFFFF, SOC UID:0xFFFFFFFFFFFFFFFF, SoC Debug:Unknown"

then i execute debug flash

S32DS return "Failed to execute MI command  py flash()"

 

can someone tell me what's happaned? 

tst_connection.jpgrst_tst_conn.jpgdebug_flash.jpg

 

0 件の賞賛
返信
3 返答(返信)

973件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you share which version of S32Design studio you are using?

Best regards,

Peter

0 件の賞賛
返信

960件の閲覧回数
devon1020
Contributor I

Hi test environment is below

1. S32DS Version: 3.6.1

2.S32K148EVB 

3.NXP S32 Debug Probe using JTAG

update:

i press reset switch while into Debug Flash

S32DS return 

"ccs:Core not responding"

 

rst_debug_flash.jpg

0 件の賞賛
返信

917件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hard to say. If you triggered reset during the programming of flash, you could possibly corrupt the Flash Config at address 0x400 and brick the device.

You can try attaching to running target or integrated PE Micro debugger if you have NXP EVB.

Also you can test it with another board / uC.

Best regards,

Peter

0 件の賞賛
返信