S32K148EVB+TJA1101 usage issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148EVB+TJA1101 usage issues

4,279 Views
Chris_Tigger
Contributor III

I have the S32K148EVB and the TJA1101 Adapter Card,prepare to learn Ethernet communication. The MCU on S32k148EVB is S32K148UA,I read the datasheet,The S32K148UJ or S32K148HJ is the products supported by Ethernet,but the kit I bought is from the official website. Could I learn Ethernet with my kit at this time?

 

Best Regards!
Chris Tigger
0 Kudos
Reply
13 Replies

4,251 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

yes, you can. I can't see any roadblock with your embodiment. You may start with lwip_s32k148 example.

Best regards,

Pavel

0 Kudos
Reply

4,235 Views
Chris_Tigger
Contributor III
There is also S32K148UA 176pin if Ethernet and SAI can be used at the same time.

Best Regards!
Best Regards!
Chris Tigger
0 Kudos
Reply

4,223 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

Yes, I think so. You can check that very easily in file S32K148_IO_Signal_Description_Input_Multiplexing.xlsx , which is an attachment of S32K1-RM.pdf.

Best regards,

Pavel

0 Kudos
Reply

4,244 Views
Chris_Tigger
Contributor III

Chris_Tiger_1-1748004204713.png

 

Thanks for your help,

As shown in the picture above.

I still have a question, the datasheet mentions that the S32K148UA series does not have Ethernet support, can I think that as long as it is S32K148 176pin, I can use Ethernet? The rules for the name of the product are not very well understood.

 

Best Regards!

Best Regards!
Chris Tigger
0 Kudos
Reply

4,225 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

I thought that all S32K148 supports ENET. But the device marking shall match as well. So, your question is absolutely correct.

My S32K148EVB-Q176 board uses UJ version.

Could you share with me the whole part number?

Could you read register SDID by a debugger and share the value? 

Best regards,

Pavel

0 Kudos
Reply

4,220 Views
Chris_Tigger
Contributor III

The part number is FS32K148UAVLU QN20V QAC1720J,I bought it from an agent, because I was afraid that I would not be able to return it, so I didn't seal it, I could only see the part number.I hope to get an answer from you, so that I can use it with peace of mind.

Chris_Tiger_0-1748008552989.jpeg

Chris_Tiger_1-1748008571762.jpeg

Best Regards!

Best Regards!
Chris Tigger
0 Kudos
Reply

4,184 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

I believe that it is OK since schematic shows UA version as well. Anyway, I'm double checking this with apps. I'll be back to you once I get a response.

Best regards,

Pavel

0 Kudos
Reply

4,140 Views
Chris_Tigger
Contributor III

I test the board in debug mode, The values of the register group can be seen in the IDE's window.Does that mean I can use the ethernet module normally?

Chris_Tiger_0-1748071601880.png

Best Regards!

Best Regards!
Chris Tigger
0 Kudos
Reply

4,182 Views
Chris_Tigger
Contributor III
Thanks very much,I pray that you can also help me test the UA version, I'm waiting for your reply online. I'm very anxious!
Best Regards!
Chris Tigger
0 Kudos
Reply

4,078 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

Could you read register SDID by a debugger and share the value?

Thank you.

Best regards,

Pavel

0 Kudos
Reply

4,068 Views
Chris_Tigger
Contributor III
I am considering purchasing a version of the S32K148UJ. The board has been returned to the agent and is currently unavailable fot testing. but I am in mainland of China, it is most convenient to buy through an agent. Look at many,basically are S32K148UA or S32K148HA,it would be best if I could get an accurate answer here.
Best Regards!
Chris Tigger
0 Kudos
Reply

4,065 Views
PavelL
NXP Employee
NXP Employee

Hello @Chris_Tigger ,

I apologize. I escalated your query, but I didn't get reply yet.

Best regards,

Pavel

0 Kudos
Reply

4,063 Views
Chris_Tigger
Contributor III
Many thanks, I will buy the kit again until Ican ensure the S32K148UA or S32K148HA has the Eth support, I am sorry for that.
Best Regards!
Chris Tigger
0 Kudos
Reply