S32K148 - OverRun on UART in debugge mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 - OverRun on UART in debugge mode

1,058件の閲覧回数
BRodriguesEBV
Contributor I

Hello,

I'm using S32K148F2M0M11. with"Libraries support" : "newLib Debugger console" and I add sometime OverRun on UART in debugge mode. Using Librarie "newLib no I/O", no more OverRun but I can't using Debugge mode. The baudrate of UART is 19200 baud. Is not hight speed. I use tool version is : S32 Design Studio : version 2.2, build 200116

Is this normal behavior? Have you ever encountered this kind of situation? Do you have a solution so that he can activate debugging again?

Thanks for your support.

0 件の賞賛
返信
1 返信

1,029件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is known limitation for UART. In debug mode received data are passed to buffer, but aren't processed if the MCU is halted. 

0 件の賞賛
返信