S32K148 LQFP Pinout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 LQFP Pinout

6,522 Views
MaxYildiz
Contributor I

Hi
I need the pinout for FS32K148UJT0VLLT
This version has 100-pin LQFP package

I can find pinout for S32K142, S32K144, S32K146 100-pin LQFP in the excel sheets attached to the reference manual. But S32K148 sheet does not include 100-pin LQFP package.

Thanks
Max

0 Kudos
Reply
3 Replies

6,512 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Max,

Would you please check the excel sheets attached to the S32K1xx MCU Family - Reference Manual (REV 13)?

S32K148_100LQFP.jpgS32K148_100LQFP.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,836 Views
ankan_creatara
Contributor III

Hi @Robin_Shen ,

The link provided by you is in pdf format. I could not find the excel sheets.

Could you kindly help me find out the excel sheet.

Thank you.

0 Kudos
Reply

5,826 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The excel sheet is in the attachment of pdf file:

attachments.pngattachments.png

0 Kudos
Reply