S32K148 EVB IAR Sample Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 EVB IAR Sample Project

5,394 Views
christhomas
Contributor II

Is there anywhere a sample start-up project in IAR Embedded Workbench to use with the S32K148EVB board.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

5,069 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

We deliver this type of project for SDK. You can get it from this path: <SDK_PATH>\examples\S32K148\demo_apps\hello_world_iar.

Best regards,

Razvan

0 Kudos
Reply

5,067 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached are some examples for IAR. Then we have application note AN5413 with examples for S32 Design Studio.

And finally there are SDK examples in S32 Design Studio:

S32 Design Studio IDE for Arm® based MCUs | NXP 

Regards,

Lukas

4,891 Views
robinseong
Contributor I

Thank you.
Do you have the latest version? (2020 year)

0 Kudos
Reply