S32K148 EVB IAR Sample Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 EVB IAR Sample Project

5,388件の閲覧回数
christhomas
Contributor II

Is there anywhere a sample start-up project in IAR Embedded Workbench to use with the S32K148EVB board.

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

5,063件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

We deliver this type of project for SDK. You can get it from this path: <SDK_PATH>\examples\S32K148\demo_apps\hello_world_iar.

Best regards,

Razvan

0 件の賞賛
返信

5,061件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached are some examples for IAR. Then we have application note AN5413 with examples for S32 Design Studio.

And finally there are SDK examples in S32 Design Studio:

S32 Design Studio IDE for Arm® based MCUs | NXP 

Regards,

Lukas

4,885件の閲覧回数
robinseong
Contributor I

Thank you.
Do you have the latest version? (2020 year)

0 件の賞賛
返信