S32K148 CAN TX Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 CAN TX Issue

2,241件の閲覧回数
gms_aditya_shuk
Contributor I

Hello,

I am facing the following issue with CAN Frame Transmission:-

- Data is properly filled in Message Buffer, but the code and time stamp is not changing and it keeps on sending data on CAN Bus and after some time bus get off.

- if Tx data is (0x55,0x55,0x55,0x55,0x55,0x55,0x55,0x55) or (0x55,0xAA,0x55,0xAA,0x55,0xAA,0x55,0xAA) the data is getting properly transmitted without any error.

I am not able to find the solution , please help me for this issue.

Thanks,

Regards,

Aditya 

タグ(2)
0 件の賞賛
返信
1 返信

2,033件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Do you have another instance on the bus that acknowledges the message? The message needs to be acknowledged, otherwise it will be resent immediately.

Regards,

Daniel

0 件の賞賛
返信