S32K148 CAN TX Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 CAN TX Issue

2,245 Views
gms_aditya_shuk
Contributor I

Hello,

I am facing the following issue with CAN Frame Transmission:-

- Data is properly filled in Message Buffer, but the code and time stamp is not changing and it keeps on sending data on CAN Bus and after some time bus get off.

- if Tx data is (0x55,0x55,0x55,0x55,0x55,0x55,0x55,0x55) or (0x55,0xAA,0x55,0xAA,0x55,0xAA,0x55,0xAA) the data is getting properly transmitted without any error.

I am not able to find the solution , please help me for this issue.

Thanks,

Regards,

Aditya 

Tags (2)
0 Kudos
Reply
1 Reply

2,037 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Do you have another instance on the bus that acknowledges the message? The message needs to be acknowledged, otherwise it will be resent immediately.

Regards,

Daniel

0 Kudos
Reply