S32K148 Board Not Powering Properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 Board Not Powering Properly

1,210件の閲覧回数
Arun07837
Contributor I

I am using S32K148 Evaluation Board for an application and Facing issue in Powering the Board

1. When we do UART TX and RX connection from Evaluation Board to TTL converter, the DS2 & DS3 LED of Evaluation board are not turning ON.

2. All the Jumper connections are made to default state. Powered the Board using USB

3. If we remove RX connection of evaluation to TX of TTL board the DS2 & DS3 LED are turning ON.

Let me know what might be the issue, how to resolve this

 

0 件の賞賛
返信
1 返信

1,195件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Arun07837

When EVB is powered from USB,LED D10 should light green,while LEDs DS2 and DS3 light orange.

Senlent_0-1639469695053.png

As you can seen from the above picture,the problem may be caused by the wiring.

 

I don’t know which pins you are using,may be you can try PTA30 & PTA29(LPUART2)

BR!

     Jim,

0 件の賞賛
返信