S32K146 Low Voltage Detect

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K146 Low Voltage Detect

跳至解决方案
3,541 次查看
kun_wang
Contributor II

hi engineer

i do not find the demo about LVD in SDK. I donot know how to code to enable the LVD function.could you help me? thank you advance. 

0 项奖励
回复
1 解答
3,458 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

It is not implemented in the SDK drivers.
If you just want to reset the MCU when VDD drops below the V_VLD threshold, you need to set the LVDRE bit.

pastedImage_1.png

pastedImage_3.png

If you need an interrupt instead of the reset.

A simple example is attached.

BR, Daniel

在原帖中查看解决方案

2 回复数
3,459 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi [email protected],

It is not implemented in the SDK drivers.
If you just want to reset the MCU when VDD drops below the V_VLD threshold, you need to set the LVDRE bit.

pastedImage_1.png

pastedImage_3.png

If you need an interrupt instead of the reset.

A simple example is attached.

BR, Daniel

3,458 次查看
kun_wang
Contributor II

thank you Daniel, it can work in my project.

i want use this function to store some important data in mcu flash.

0 项奖励
回复