S32K144EVB gerber file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB gerber file

Jump to solution
3,063 Views
remco1
Contributor I

Hello,

I'm trying to design a shield for the S32K144EVB.

However, the board file on the website cannot be opened in Eagle (download the latest version).

At the moment I don't know how to place to connectors to matchup with the board.

Are there gerber files available so I can finish my shield design?

Kind regards,

Remco de Wit

1 Solution
2,882 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Remco de Wit,

I just sent you the Gerber files to your email, please confirm if you receive them.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
8 Replies
1,403 Views
maxtan
Contributor I

I need a gerber file, too.
Can you send it?

0 Kudos
Reply
2,018 Views
akshay_aggarwal1305
Contributor I

Hello,

 Please share the gerber files for S32k144EVB kit as we are using eagle software to design the compatible shield. 

 

Awaiting for a quick response. 

Regards,

Akshay

0 Kudos
Reply
2,882 Views
a01224960
Contributor I

Hello,

I am dealing with the same kind of problem, but intstead I am using the S32K148EVB.

Would it be possible to get those files too?(I am also using eagle to design a shield).

Thank you

0 Kudos
Reply
2,882 Views
remco1
Contributor I

Hello,

Thank you for the gerber files. I have received them. 

Kind regards,

Remco de Wit

2,882 Views
adonai1
Contributor I

I need a gerber file, too.
Can you send it?

Thanks.

0 Kudos
Reply
2,883 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Remco de Wit,

I just sent you the Gerber files to your email, please confirm if you receive them.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,384 Views
BambooTu
Contributor I

I posted this question in the thread:

https://community.nxp.com/t5/S32K/S32K144EVB-gerber-file/m-p/1770749/emcs_t/S2h8ZW1haWx8YWNjZXB0X2Fz...

Could you please let me know if it's possible to send the Gerber File for the development board via email?

0 Kudos
Reply
2,825 Views
Guinnpartners
Contributor I

Please share gerber files and parts lists so we can get organized on component sourcing given long lead times for our custom PCB project based on the S32K144 EVB as well.

 

0 Kudos
Reply