Hi,
I'm trying out the secure boot feature on the S32K144EVB board. I'm being careful, as I don't want to brick the board. I'm seeing two different options for boot size:
1. In the sample code provided in AN5401SW, example #4 shows how to configure secure boot manually. It sets the BOOT_SIZE to 128*1024*8.
2. In the SDK code for CSEC module provided by Processor Expert, the comments indicate the bootSize is the number of blocks of 128-bit data to check on boot. Maximum size is 512KB.
Based on (2), would the maximum bootSize be equals to (512KB / 128bit) = 4096?
But in (1), the BOOT_SIZE is defined as 128*1024*8 = 1,048,576.
What is the correct way to calculate the boot size?
Thanks!