Can i trigger ADC0 through PDB0 Channel 0 and ADC1 through PDB0 Channel 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i trigger ADC0 through PDB0 Channel 0 and ADC1 through PDB0 Channel 1

1,716 Views
nitinverma
Contributor III

Hi support Team,

 

I am using  SD32K144 eval board.I wanted to use ADC0,ADC1 simultaneously in back to back to mode.I wanted to trigger ADC0 through PDB0 Channel0 and ADC1 through PDB0 Channel 1 in back to back mode.8 channel of ADC0 is working perfectly but Adc1 is not working kindly help me 

Below is the code for PDB and ADC initialization.

void PDB_Init(void)
{
PCC->PCCn[PCC_PDB0_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable bus clock in PDB0 */

PDB0->SC |= PDB_SC_TRGSEL(0xF) | /* b1111: Software trigger is selected */
PDB_SC_PRESCALER(1) | /* Prescaler: 010 = sysclck/(2*MULT) = 80 / (2*1) = 40MHz */
PDB_SC_MULT(0) | /* 00: Multiplication factor is 1. */
PDB_SC_PDBEN_MASK; /* 1: PDB enabled */
PDB0->CH[0].C1 |= PDB_C1_BB(0xFE) | /* DLY[0] : pre-trigger from PDB DLY */
/* DLY[7:1] : back-to-back enabled */
PDB_C1_TOS(0x00) | /* Pretrigger Output Select: 0=bypassed , 1=enabled */
PDB_C1_EN(0xff); /* PDB channel's [3:0] pre-trigger enabled */


PDB0->CH[1].C1 |= PDB_C1_BB(0x03) | /* DLY[0] : pre-trigger from PDB DLY */
/* DLY[3:1] : back-to-back enabled */
PDB_C1_TOS(0x00) | /* Pretrigger Output Select: 0=bypassed , 1=enabled */
PDB_C1_EN(0x03); /* PDB channel's [3:0] pre-trigger enabled */

// PDB0->MOD = 2200;
// PDB0->IDLY = 2200;
// PDB0->CH[0].DLY[0] = 100; /* Pretrigger 0 : 100 * 25e-9 = 2.5e-6 */
PDB0->SC |= PDB_SC_LDOK_MASK;

 

}

void ADC_Init(void)
{

/* ADC0 configuration */
PCC->PCCn[PCC_ADC0_INDEX] &= ~PCC_PCCn_CGC_MASK; /* Disable clock to change PCS */
PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_PCS(6); /* PCS=3: Select SPLL */
PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable bus clock in ADC */

 


ADC0->CFG1 |= ADC_CFG1_ADICLK(0) | /* Only ALTCLK1 is available */
ADC_CFG1_ADIV(2) | /* the clock rate is (input clock)/4 */
ADC_CFG1_MODE(1); /* 0b00: 8-bit, 0b01: 12-bit, 0b10: 10-bit */
ADC0->SC2 |= ADC_SC2_ADTRG(1); /* Conversion Trigger: 0b0= SW , 0b1 = HW */
ADC0->SC3 |= ADC_SC3_AVGE(1)|ADC_SC3_AVGS(3);

ADC0->SC1[0] = ADC_SC1_ADCH(12); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[1] = ADC_SC1_ADCH(13); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[2] = ADC_SC1_ADCH(0); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[3] = ADC_SC1_ADCH(6); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[4] = ADC_SC1_ADCH(8); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[5] = ADC_SC1_ADCH(9); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[6] = ADC_SC1_ADCH(2); /* Select AD12 (ADC0_SE12) @PTC14 */
ADC0->SC1[7] = ADC_SC1_ADCH(5); /* Select AD12 (ADC0_SE12) @PTC14 */


PCC->PCCn[PCC_ADC1_INDEX] &= ~PCC_PCCn_CGC_MASK; /* Disable clock to change PCS */
PCC->PCCn[PCC_ADC1_INDEX] |= PCC_PCCn_PCS(6); /* PCS=3: Select SPLL */
PCC->PCCn[PCC_ADC1_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable bus clock in ADC */

 

/* ADC1 configuration */
ADC1->CFG1 |= ADC_CFG1_ADICLK(0) | /* Only ALTCLK1 is available */
ADC_CFG1_ADIV(2) | /* the clock rate is (input clock)/4 */
ADC_CFG1_MODE(1); /* 0b00: 8-bit, 0b01: 12-bit, 0b10: 10-bit */
ADC1->SC2 |= ADC_SC2_ADTRG(1); /* Conversion Trigger: 0b0= SW , 0b1 = HW */
ADC1->SC3 |= ADC_SC3_AVGE(1)|ADC_SC3_AVGS(3);

ADC1->SC1[0] = ADC_SC1_ADCH(10); /* Select AD12 (ADC1_SE10) @PTC14 */
ADC1->SC1[0] = ADC_SC1_ADCH(2); /* Select AD12 (ADC0_SE2) @PTC14 */
}

Thanks

Nitin verma

Labels (1)
0 Kudos
Reply
3 Replies

1,147 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

to do simultaneous conversion on both ADC0 and ADC1 you have to trigger ADC by PDB0 and ADC1 by PDB1. Both PBDs can be triggered by the same source from the TRGMUX.

pastedImage_1.png

attached is simple code to do two simultaneous conversions on ADC0 and ADC1. Software trigger is used to start conversion.

BR, Petr

0 Kudos
Reply

1,147 Views
gumpforrest
Contributor I

Hi !

Can you show this function with SDK configuration tool ?

That is, muti-channals in both ADC0 and ADC1 trigged by PDB0 and PDB1

I suppose SDK will be used mostly in future...

Thanks a lot !

0 Kudos
Reply

1,147 Views
nitinverma
Contributor III

Thanks a lot petr

BR, Nitin

0 Kudos
Reply