Hi NXP support:
I have encountered a problem when configuring the HSRUN mode in S32K144 that the picture shows below indicates HSRUN mode can be entered through two way: with 112MHZ SPLL or with 80MHZ.So I want to know if I choose 80MHZ SPLL as clock source, what's the difference with RUN mode in 80MHZ?(Besides HSRUN mode can not operate flash.) And whether HSRUN mode with 80MHZ clock will work in 112MHZ?
Best regards
Bill wu
Hi @BillWu123,
You can find chapter 40.4.3.3 High Speed Run (HSRUN) mode from S32K1 Reference Manual. The main difference in HSRUN, the on-chip voltage regulator remains in a run regulation state, but with a slightly elevated voltage output. In this state, the MCU is able to operate at a faster frequency compared to normal RUN mode. For the maximum allowable frequencies, see the Power Management chapter.
Also, in this chapter, the restrictions for HSRUN are mentioned:
To enter HSRUN mode (with 112 MHz SPLL as clock source):
Best regards,
Julián