S32K144 Q100 openSDA application issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Q100 openSDA application issue.

1,288 Views
sjshin
Contributor I

hi,

I'm trying to download a bin file from a vendor to my S32K144 development board.
So, after making a USB connection between S32K144 <-> PC, I copied that BIN file to the S32K144 folder.

However, the OPENSDA LED blinked 8 times and then turned off for 2 seconds.
According to the OPENSDAUG file, this is an error phenomenon.

How can I install the bin file normally without this problem?

Thanks.

0 Kudos
Reply
1 Reply

1,269 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to the discussion in S32K144 D2 RED LED is ON always 

If your computer is Win10, please Disable/stop Windows Services by refer to Recovering OpenSDA Boards with Windows 10


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply