S32K144 Pin-Outs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Pin-Outs

12,928 Views
andyfraser
Contributor I

I am hoping to use the S32K144 64-pin device in the near future and thought I would create a schematic symbol for it. However, I am having difficulty locating the pin-out diagram. In the S32K1XX datasheet it says "For package pinouts and signal descriptions, refer to the Reference Manual." and in the Reference Manual is says "See IO Signal Description Input Multiplexing sheet(s) attached to the Reference Manual for pinout diagrams corresponding to available packages.".

So, where are the pin-outs ?!

Andy

3 Replies

8,735 Views
isaaclee
Contributor I

Is there any reason why you put the document as an attachment instead of putting it in the same document?
It seems a bit inconvenient for the viewer only.

0 Kudos
Reply

10,393 Views
andyfraser
Contributor I

Daniel,

Many thanks - I did not realize that you can attach files to a PDF !

Thanks again.

Andy

10,393 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi

 

You can find the latest RM Rev3 on the product page.

The pin out is then in the attachments:

RM_attachements.png

Regards

Daniel