S32K144 LPSPI Transfer in 16bit mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 LPSPI Transfer in 16bit mode

1,858件の閲覧回数
phanendravarma_
Contributor II

Hello ,

I configured LPSPI Driver to transmit some dummy 16bit data on MOSI and its working(measured on CRO).

I have one doubt with respect to MISO capture?Is LPSPI will support Full duplex communication means in one instance i can put the data on MOSI and as well as i can read data on MISO?

or in First instance(16 clocks) i need to send data and in next instance(16clocks), i must read data on MISO?

Actually, I want to establish LPSPI 16bit communication with SBC(FS45xx).

Thank you.

タグ(2)
0 件の賞賛
返信
1 返信

1,716件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Yes, the LPSPI support full-duplex mode, simultaneous transfers in both directions. 

Regards,

Daniel

0 件の賞賛
返信