S32K144 Internal clock settings using clock config tool in S32 DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Internal clock settings using clock config tool in S32 DS

Jump to solution
1,350 Views
emb02
Contributor IV

Hi,

I'm using S32K144 controller with internal oscillator and I want to set system clock to 80MHz using clock config tool.

I've referred RF manual in which internal clock settings are given for normal run mode but I'm not able to set clock. Also I've noticed some difference in Clock diagram in RF manual and clock config tool in S32DS, can I get explanation for this?

I'm attaching clock settings image for reference. Please help me with this.

I'm using S32DS v 3.5.

 

Regards, 

EMB02

Tags (2)
0 Kudos
Reply
1 Solution
1,330 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Note: Available only in S32K14xW as indicated in YELLOW.
This is the reason that you can not select FIRC as clock source of SPLL.

Available only in S32K14xW as indicated in YELLOW.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,331 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Note: Available only in S32K14xW as indicated in YELLOW.
This is the reason that you can not select FIRC as clock source of SPLL.

Available only in S32K14xW as indicated in YELLOW.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,321 Views
emb02
Contributor IV
Hi,
Thanks for help.

Regards
EMB02
0 Kudos
Reply