Hi,
I'm using S32K144 controller with internal oscillator and I want to set system clock to 80MHz using clock config tool.
I've referred RF manual in which internal clock settings are given for normal run mode but I'm not able to set clock. Also I've noticed some difference in Clock diagram in RF manual and clock config tool in S32DS, can I get explanation for this?
I'm attaching clock settings image for reference. Please help me with this.
I'm using S32DS v 3.5.
Regards,
EMB02
已解决! 转到解答。
Hi
Note: Available only in S32K14xW as indicated in YELLOW.
This is the reason that you can not select FIRC as clock source of SPLL.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
Note: Available only in S32K14xW as indicated in YELLOW.
This is the reason that you can not select FIRC as clock source of SPLL.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------