S32K144 IO output level changed issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 IO output level changed issue

888 Views
Ali22
Contributor III

Dears

I encounter an issue like this: when I do S32K144 CAN BUS-OFF experiment, I put an IO toggle function in the CAN error interrupt to indicate CAN BUS-OFF happened,  MCU VDD supply is 5V, but when I view the  IO toggle output waveform I found sometimes the IO output level changed to about 3.5V, in the meanwhile VDD 5V is no change, so I get confused why the output changed to 3.5V in sometimes? I confirm there is no reset happened when 3.5V come out, and 3.5V pulse width is about 10ms, it doesn't seems like a noise,  dose K144 entry to a special mode that may cause the output level changed?Anyone who meet this kind of issue, thanks.

1.jpg2.jpg

 

0 Kudos
Reply
1 Reply

863 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ali22

Please provide a simple project that can reproduce the problem, I will help you test and analyze it.

0 Kudos
Reply